VBUS.RMSLIMIT
Description
This parameter reads the limit of the bus capacitor load. When the bus capacitor loads exceeds this limit, the drive generates fault F503.
Excessive bus capacitor load may indicate a disconnected main supply phase.
General Information
Type |
R/O Parameter |
Units |
Vrms rms stands for root mean square (also known as the quadratic mean) |
Range |
N/A |
Default Value |
N/A |
Data Type |
Integer |
See Also |
N/A |
Start Version |
M_01-00-00-000 |
Related Topics