VBUS.UVWTHRESH

Description

If VBUS.VALUE value drops below VBUS.UVWTHRESH, then a warning is generated.

General Information

Type

NV Parameter

Units

VDC

Range

0 to 900 VDC

Default Value

10 volts above the default value of the under voltage fault threshold (VBUS.UVFTHRESH). The default value of VBUS.UVFTHRESH is hardware dependent.

Data Type

U16

See Also

VBUS.UVFTHRESH

Start Version

M_01-00-00-000

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3495h/0

M_01-00-00-000

Related Topics

Regeneration