VL.KO

Description

VL.KO is used to scale the observer model to match the load. When VL.KO is tuned properly, VL.MODEL will match VL.FB , except when there is an unspecified offset between the two.

General Information

Type

R/W Parameter

Units

Internal

Range

0 to 65,535

Default Value

0

Data Type

Float

See Also

VL.MODEL

Start Version

M_01-00-01-000

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

51B3h/0

M_01-00-01-000

Related Topics

Velocity Loop