ACTION#.SOURCETEXT
Description
This parameter defines the text associated with an ACTION Source.
To clear the text stored, use issue: ACTION#.SOURCETEXT clear to remove the text and commands.
Action Sources Using SOURCETEXT:
- 26: Recordable Parameter – see 26 – Recordable Parameter.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-05-01-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
|
|
Data Type |
String |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported