AXIS#.SAFEPARAM.STO​.RESTARTACKMODE

Description

Indicates whether the Safe TorqueClosed Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist Off (STO) will automatically reset or requires a manual reset using safe input or FSoE. In Automatic Restart mode, when the STO input clears, the STO automatically restarts and the drive is enabled. In Manual Restart mode, when the STO input clears, the STO remains active until the configured input triggers the STO to restart. See AXIS#.SAFEPARAM.STO​.RESTARTACKSOURCE).

Value Description

0

Automatic Restart (default)

1

Manual Restart

 

Context

For complete STO information refer to STO (Safe Torque Off).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-01-02-000

General Information

Type

Read/Write

Units

N/A

Range

0 (Automatic Restart)
1 (Manual Restart)

Default Value

0 (Automatic Restart)

Data Type

Integer

Stored in Non Volatile Memory

No