AXIS#.SAFEPARAM.STO​.RESTARTACKSOURCE

Description

Indicates the input to use to manually clear the Safe TorqueClosed Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist Off (STO) once the STO input is cleared. Only used when the STO is configured for Manual Restart mode (see AXIS#.SAFEPARAM.STO​.RESTARTACKMODE).

 

Value Description

0

Not Used

1

Safe Input 1

2

Safe Input 2

3

Safe Input 3

4

Safe Input 4

5

Safe dual input 1

6

Safe dual input 2

 

Context

For complete STO information refer to STO (Safe Torque Off).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-01-02-000

General Information

Type

Read/Write

Units

N/A

Range

0 or 6

Default Value

0 (Not used)

Data Type

Integer

Stored in Non Volatile Memory

No