Structured Text (ST) / Instruction List (IL) Editor
"Structured text"
A high-level language that is block structured and syntactically resembles Pascal / IL
"Instruction list"
This is a low-level language and resembles assembly editor is a language-sensitive text editor dedicated to IEC
"International Electrotechnical Commission"
IEC is a not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies 61131-3 languages.
The editor supports advanced graphic features such as drag-and-drop, syntax coloring, and active tooltips for efficient input and test of programs in ST and IL.
Related Sections
- Auto-completion of Words
- Bookmarks
- Read the Output of a MC Function Block in ST
- Select Variables and Instances
- Select function blocks
- ST / IL Drag-and-Drop
- ST / IL Language Selection
- ST / IL Syntax Coloring
- Tooltips in the ST / IL Editor
-
-
Press Ctrl + Spacebar to open the Variable Editor dialog box.