Timers

These are the standard functions for managing timers:

FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. Description
BLINK

Blinker

BlinkA

Asymmetric blinker

PLS

PulseClosed When the step gets activated, the action is activated for a single execution, and possibly once again when the step is deactivated signal generator

TMD

Down-counting stop watch

TMU / TMUsec

Up-counting stop watch (seconds)

TOF / TOFR

Off timer

TON

On timer

TP / TPR

Pulse timer

These functions make use of the Time data type.

See Data Types for more information.