Glossary
Terms in this Glossary are provided for informational purposes only and can describe features not included in your particular license.
|
Term |
Definition |
|
Actuator |
A mechanical device for moving or controlling a mechanism or system. An actuator is typically a mechanical device which transforms an input signal (usually an electrical signal) into motion. |
|
Bandwidth |
In computer networking, bandwidth refers to a data rate measured in bits per second (e.g., network throughput). The limit to the data rate of a physical communication link is related to its bandwidth in hertz. |
|
Black Channel |
A black channel
|
|
Cam Profiling |
The position of a slave axis is mathematically linked to the position of a master axis.
|
|
CANopen |
CANopen is a communication protocol and device profile specification for embedded systems used in automation for fieldbuses See CANopen. |
|
Casting |
See Typecasting. |
|
Closed Loop |
The use of feedback devices (i.e., encoders, resolvers, interferometers, etc.) to allow a motor to position a user payload accurately. |
|
COM |
COM is the original name of the serial port interface. It refers to physical ports and virtual ports (e.g., ports created by bluetooth or USB |
|
Contactor |
An electrically controlled switch (relay) used for switching a power circuit.
|
|
The difference between the configured cycle time and the actual measured cycle time. Units are in microseconds. |
|
|
A basic transfer unit in which the delivery arrival time and order are not guaranteed.
|
|
|
DeviceNet |
A communication protocol (based on Controller Area Network) used in the automation industry to interconnect control devices for data exchange. Typical applications are information exchange, safety devices, and large I/O control networks. |
|
Drive |
In electrical engineering, a drive is an electronic device providing power to a servo or stepper motor, and controlling it through the current and timing in its coils |
|
Driver |
In computing and electronics, a driver is a software component allowing higher-level computer programs to interact with a computer hardware device. A driver typically communicates with the device through the computer bus or communications subsystem to which the hardware is connected. |
|
Big-endian and little-endian describe the order a sequence of bytes are stored in computer memory.
Example: The decimal integer 56789652 (0x03628a94 in hexadecimal) is stored as:
KAS applications can be downloaded to big-endian or little-endian processor targets. |
|
|
Environment Objects |
Global objects that exist before the execution of the script. Typically, they are global objects of the KAS-IDE |
|
EtherCAT |
Ethernet
See EtherCAT. |
|
Ethernet |
A large, diverse family of frame-based computer networking technologies that operate at many speeds for local area networks (LANs). |
|
EtherNet/IP |
An open industrial application layer protocol for industrial automation applications. |
|
The inputs are taken into account at each cycle depending on the system Periodicity (for example each millisecond).
|
|
|
Feedback Device |
|
|
Feed-forward |
Describes an element or pathway within a control system which passes a controlling signal from a source in the control system's external environment. Often a command signal from an external operator to a load elsewhere in its external environment. |
|
An industrial network protocol used for distributed control (e.g., EtherCAT, CAN It is a way of connecting instruments in a plant design. |
|
|
A non-volatile computer storage chip that can be electrically erased and reprogrammed.
|
|
|
Frame |
In networking dialect, a message is called a frame. |
|
Front-end |
In software design, the front-end is the part of a software system that interacts directly with the user. |
|
Homing |
The homing procedure allows a position offset to the motor in order to ensure it is physically at the home position.
|
|
Interrupt |
An asynchronous signal from hardware indicating the need for attention or a synchronous event in software indicating the need for a change in execution. |
|
Jerk |
In physics, this is the rate of change of acceleration. More precisely, the derivative of acceleration with respect to time. |
|
Latch |
The control word is used to activate the drive's latch status machine.
|
|
MAC address |
Media Access Control address
|
|
ModBus |
A serial communications protocol and the most commonly available means of connecting industrial electronic devices.
|
|
Motion Bus |
An industrial network protocol used for real-time distributed control (e.g., EtherCAT). |
|
Motion control |
A sub-field of automation, in which the position and/or velocity of machines are controlled using some type of device such as a hydraulic pump, linear actuator
|
|
Motor |
An actuator focused to a movement, converting electrical energy in a force or torque |
|
Non-volatile |
Information is stored in a specific memory to remain accessible even when the application has been powered off. |
|
Online Change |
Applies to downloading PLC |
|
Online Configuration Mode |
Applies to EtherCAT communication to the drives in a special mode. |
|
Open Loop |
A positioning technique, typically utilizing stepper motors, in which the controller issues a sequence of commands to the motor without any absolute means of detecting if the move has in fact been made. When the load and move velocity and acceleration are appropriately defined, open loop |
|
OpenGL |
Open Graphics Library A standard specification defining a cross-language, cross-platform API for writing applications that produce 2D and 3D computer graphics. The Softscope uses this API to implement graphical manipulations. |
|
A specification of a CPU whose instructions are expected to be executed in software rather than in hardware.
|
|
|
The period of execution of a pipe is the time spent between two successive computations of set values for the same pipe. The period of execution of a pipe is specified by the PERIOD parameter of the input Pipe Block. |
|
|
PLCopen |
A vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML |
|
Pragma |
A compiler directive communicating additional pragmatic information.
|
|
Precedence |
In arithmetic and algebra, when a number or expression is both preceded and followed by a binary operation, a rule is required for which operation must be applied first.
|
|
Probe |
See Softscope - Probe. |
|
Pulse |
When the step gets activated, the action is activated for a single execution, and possibly once again when the step is deactivated. |
|
Reference Counting |
In computer science, this is a technique of storing the number of references, pointers, or handles to a resource such as an object or block of memory. It is used as a means of de-allocating objects which are no longer referenced. |
|
The transition of a digital signal from low to high. AKA: positive edge. |
|
|
Run-time |
In computer science, run-time (or run time |
|
Sensor |
A type of transducer that converts one type of energy into another for various purposes including measurement or information transfer |
|
Service Port |
UDP
|
|
A special electric amplifier used to power electric servo motors. It monitors feedback signals from the motor and continually adjusts for deviation from expected behavior. |
|
|
Setpoint |
The target value that an automatic control system (e.g., a PID |
|
Softscope - Channel |
A channel is used by the softscope to acquire the evolution of a variable which is plugged on it. |
|
A device that uses onboard instruments to gather and relay a variety of measurement to controllers from remote locations. Probes can return their data over radio links or be physically tethered to controllers or another device, or to collect and return physical samples. |
|
|
Softscope - Sampling |
To acquire the variable's evolution, samples are taken at fixed intervals. The accuracy to create the trace depends on the resolution of the acquisition. The sampling frequency must be higher than 2 times the highest frequency in the input signal. It is called the Nyquist frequency. Theoretically it is possible to reconstruct the input signal with more than 2 samples per period. In practice, 10 to 20 samples per period are recommended to be able to examine the signal thoroughly |
|
Softscope - Time-base |
The time-base allows you to set the speed at which all the lines for each channel are drawn, and is calibrated in milliseconds per division |
|
Softscope - Trace |
The trace is the resulting graph of a variable's evolution against time, with the more distant past on the left and the more recent past on the right |
|
Stepper Drive |
A stepper drive is a special electric amplifier used to power electric stepper motors without position feedback (open-loop). It controls the current to the various phases in a stepper motor to control the motor’s position. |
|
Synchronization |
Combines an axis or axes group (as slave) with an axis as master so that the slave executes its path with synchronization to the progress of the master, meaning linked to a one-dimensional source for synchronization |
|
SynqNet |
SynqNet is a digital machine control network. Built on the 100BT physical layer, SynqNet provides a synchronous real-time connection between motion controllers, servo drives, stepper drives, I/O modules, and custom devices |
|
In the HMI |
|
|
A timestamp is a sequence of characters denoting the date and/or time at which a certain event occurred |
|
|
Torque |
Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist. The SI unit for torque is the newton metre (N.m). |
|
In computer science, type conversion or typecasting |