ECATGetObjVal
-
-
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Deprecated as of KAS v2.7.
The recommended best practice is to map a PLC
"Programmable Logic Controller"
A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines.
Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events variable to a PDO
PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. object.