USB Flash Drive Path Conventions

Access to the USBClosed "Universal Serial Bus" USB is a serial bus standard to interface devices flash drive memory requires that a valid USB flash drive label be used at the beginning of the path, followed by the relative path to the USB flash drive.

(Valid USB Flash Drive Label)/(Relative Path)
  • A valid USB flash drive relative path starts with //, /, \\, or \.
  • This is immediately followed by usbflash which is followed by \ or /.
  • This path label is case insensitive.

The usbflash folder is created inside the userdata folder to maintain compatibility with the Simulator.

File access points to userdata/usbflash when a PCMM2G usbflash path is used on the Simulator.

Valid Paths

Valid Paths

Notes

//usbflash/file1

 

\usbflash/dir1/file1

dir1 must have been already created.

/usbflash/dir1/file1

dir1 must have been already created.

//usbflash\file1

 

Invalid Paths

Invalid Paths

Invalid Reason

///usbflash/file1

Started with more than two forward or two backward slashes.

/\usbflash/dir1/file1

Started with one forward and one backward slash.

/usbflashdir1/file1

No forward or backward slash.

/ubflash1/dir1/file1

Invalid label.

See Also