MCFB_AKDFaultLookup
Function Block
A function block groups an algorithm and a set of private data. It has inputs and outputs. - String message of the corresponding AKD drive fault number.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
EN |
BOOL |
0, 1 |
N/A |
No default |
Used in the FFLD |
|
FaultNumber |
DINT |
No range |
N/A |
No default |
The AKD drive fault number. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
OK |
BOOL |
0, 1 |
N/A |
TRUE if there is a match for the FaultNumber. |
|
FaultDescription |
STRING |
N/A |
N/A |
Description of the fault. |
Remarks
- This function or function block can be used with PLCopen
A vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML Motion engines. - The FaultNumber is the same number as reported on the display of the AKD drive.
- OK output turns TRUE when the there is a match for the FaultNumber.
- The FaultDescription displays the corresponding text string.
This image shows the function or function block I/O.
Figure 6-93: MCFB_AKDFaultLookup
Usage
- Provide drive fault information the application program uses to determine next steps.
- Example: Perform a machine-controlled stop or perform an immediate disable of the servo drives.
- In the application program, sends output fault information from this UDFB to the HMI
"Human-machine interfaces "
Also known as computer-human interfaces (CHI), and formerly known as man-machine interfaces, they are usually employed to communicate with PLCs and other computers, such as entering and monitoring temperatures or pressures for further automated control or emergency response for review by the machine operator.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Execute and Read the Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. Block
Inst_MCFB_AKDFault( Axis1(*lib:AXIS_REF*) );
FaultDrive1 := Inst_MCFB_AKDFault.FAULT;
FaultDrive1Number := Inst_MCFB_AKDFault.FaultNumber;
FaultDrive1Description := MCFB_AKDFaultLookup( FaultDrive1Number(*DINT*) );
See Also
- FB_AKDFltRpt
- MC_ReadStatus (PLCopen Motion Engine)
- MCFB_AKDFault