MCFB_ECATRestart
Function Block
A function block groups an algorithm and a set of private data. It has inputs and outputs. - Reinitializes the EtherCAT
***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs network and the motion engine.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
iEN |
BOOL |
0, 1 |
N/A |
No default |
Used in the FFLD |
|
iRSTERR |
BOOL |
1, 256 |
0, 1 |
No default |
Clears the motion engine and EtherCAT network errors in case of any faults. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
oOK |
BOOL |
0, 1 |
N/A |
Function |
|
oDONE |
BOOL |
0, 1 |
N/A |
Execution complete. |
|
oERR |
BOOL |
0, 1 |
N/A |
TRUE if the system initialization fails. |
Remarks
- This function block clears motion engine errors, motion bus driver errors and EtherCAT network errors before reinitializing the motion engine, if requested to do so.
- This UDFB allows the EtherCAT and motion engines to restart without having to restart the entire project.
Examples:
- EtherCAT network wire is replaced or accidentally disconnected.
- Axis setup parameters defined by CreateAxis and/or InitAxis function need to be changed while the application is running.
This image shows the function or function block I/O.
Figure 6-95: MCFB_ECATRestart
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
Inst_MCFB_ECATRestart( Restart, ResetErrors );
IF Inst_MCFB_ECATRestart.oDONE THEN
RestartComplte:=1;
End_IF;
See Also