MLFB_PlsTimeFw
Function Block
A function block groups an algorithm and a set of private data. It has inputs and outputs. - Forward/backward Position/Time range indicator.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
ibExecute |
BOOL |
|
|
|
Enable PLS. |
|
iDedicatedCmpID |
DINT |
|
|
|
ID of the dedicated comparator. |
|
iStartPos |
LREAL |
|
|
|
Start position of PLS. |
|
iOnTime |
TIME |
|
|
|
Time the PLS is on. |
|
iDelayTime |
TIME |
|
|
|
Delay time for compensation. |
|
ibForce |
BOOL |
|
|
|
Force PLS. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
oPLS |
BOOL |
|
N/A |
Position limit switch. |
Remarks
- Used in the command position path with ascending position.
- A dedicated comparator pipe block is needed.
- The Boolean output oPLS is set to:
- TRUE if the position has crossed the start position.
- A timer with iOnTime must be started.
- When the timer has expired the output is set to FALSE.
- TRUE if the position has crossed the start position.
- The function block is executed cyclically.
- The modulo position is considered.
- The function block has the possibility to compensate a delay time of the connected device (e.g., glue nozzles).
Timing
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//PLSOutput is True when chosen comparator passes 180 for 3 seconds a T#2ms delay
//Can also force the output to be true with ForceOuput variable
Inst_MLFB_PlsTimeFw( EnablePLS, PipeNetwork.COMPARATOR, 180, T#3s, T#2ms, ForceOutput );
PLSOutput := Inst_MLFB_PlsTimeFw.oPLS;