PipeNetwork_FFLD - Special FFLD Function
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Calls the PNCode function block in FFLD
"Free Form Ladder Diagram" POUs.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
En |
BOOL |
0, 1 |
N/A |
No default |
Request to initialize the Pipe Network. |
|
cmdID |
DINT |
N/A |
N/A |
No default |
Commands used to start and initialize the Pipe Network.
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
OK |
BOOL |
|
N/A |
Returns TRUE when the function successfully executes. |
Remarks
- It starts and initializes the Pipe Network, based on the command specified by cmdID.
- Internally this function calls the Function Block
A function block groups an algorithm and a set of private data. It has inputs and outputs. PNCode.
- Internally this function calls the Function Block
- This is a special function.
- It should only be used in Pipe Network applications that contain FFLD POUs that call PNCode.
- To use this function, Pipe Network must be declared as a global variable in the dictionary.
- Calling this function instead of PNCode in FFLD POUs eliminates this compile error that occurs after modifying the Pipe Network using the Pipe Network editor:
Controller:PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events:Main: NW1(1,14): PNCode: Invalid block height
- The compile error is generated because the number of outputs on PNCode can vary.
- This occurs after modifying the original Pipe Network using the Pipe Network editor.
- The new PNCode Function Block is not automatically updated in any FFLD POUs, reflecting the new outputs.
- Manually update each PNCode function block call in any FFLD POUs to correct this problem.
-
-
The Pipe Network FFLD Application Template is a good example of how to use this Function.
See Pipe Network 2-Axes Template - FFLD.
Figure 6-112: PipeNetwork_FFLD
FBD Language Example
Not available.
FFLD Language Example
IL Language Example
Not available.
ST Language Example
Not available.
See Also