MLAxisAddress
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Returns the motion bus address of the axis.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
ID |
DINT |
No range |
N/A |
No default |
ID Name of the Axis block. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
OK |
BOOL |
|
|
Returns TRUE when the function successfully executes. |
|
Default (.Q) |
DINT |
|
|
Returns the motion bus address of the axis. |
Remarks
- Axes have the same address when they are mapped to the same multi-axis drive (e.g., the dual-axis AKD2G drive).
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
Axis1_Address := MLAxisAddress(PipeNetwork.AXIS1);