MLAxisWriteModPos
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Sets the value period of the axis.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
AxisID |
DINT |
No range |
N/A |
No default |
ID Name of the Axis block. |
|
ModuloPosition |
LREAL |
No range |
User units |
No default |
Sets the Axis Period Value when Mode is set to Modulo. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
No range |
N/A |
Returns TRUE when the function successfully executes. See Pipe Network - General Rules for more information. |
Remarks
None
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLAxisWriteModPos(PipeNetwork.Axis1, 360) ) ;