MLPrfReadOOffset
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Returns the Output Offset value of a selected CAM Profile.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
ProfileID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of an initialized CAM Profile. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Offset |
LREAL |
|
|
Returns the Output Offset of the selected CAM Profile. |
Remarks
- Offsets can be changed on the fly to modify the CAM Profile while maintaining its shape.
- A change in output offset is equivalent to shifting the CAM Profile on the Y (or Output) Axis.
Figure 6-173: MLPrfReadOOffset
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Save value of output offset
CamOffset := MLPrfReadOOffset( Profiles.Profile_A );
See Also