MLPrfWriteIOffset
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Sets the Input Offset value of a selected CAM Profile.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
ProfileID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of an initialized CAM Profile. |
|
Offset |
LREAL |
No range |
N/A |
No default |
Desired new value of Input Offset. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
|
|
Returns TRUE if the Input Offset is changed to the new value. See Pipe Network - General Rules for more information. |
Remarks
- Offsets can be changed on the fly to modify the CAM Profile while maintaining its shape.
- A change in input offset is equivalent to shifting the CAM Profile on the X (or Input) Axis.
Figure 6-175: MLPrfWriteIOffset
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Change the value of input offset
MLPrfWriteIOffset( Profiles.Profile_A , 45 );
See Also