MLDelayInit
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Initializes a delay object.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of a created Pipe Block. |
|
CycleDelay |
DINT |
0, 9 |
Cycle |
0 (zero)) |
Number of delay cycles. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
Remarks
- This is automatically created in the compiled code of a Pipe Network.
- It is included in the MLPN_CREATE_OBJECT (created in ST
"Structured text"
A high-level language that is block structured and syntactically resembles Pascal) which is typically executed in a project as part of the startup sequence of the Pipe Network.
- It is included in the MLPN_CREATE_OBJECT (created in ST
- Returns TRUE if the function succeeded.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLDelayInit(PipeNetwork.DELAY1, 2 );