MLSyncStop
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - De-synchronizes a synchronizer Pipe Block.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Position |
LREAL |
No range |
User units |
No default |
Motion Stop Position. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
|
N/A |
Function block executed successfully. See Pipe Network - General Rules for more information. |
Remarks
Returns TRUE if the function succeeded.
Figure 6-200: MLSyncStop
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLSyncStop( PipeNetwork.SYN , 120 );