MLTrigReadPos
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Returns the position of the block at the moment when it was triggered.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of an initiated Trigger object. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Position |
LREAL |
No range |
User units |
Returns the position of the selected block's Axis at the moment when it was triggered. |
Remarks
-
-
This function or function block returns cached data.
See Program a Multi-Core Controller for more information.
- Returns the modulo-applied position of the pipe at the moment it is triggered by the Trigger Block's selected Fast Input
The inputs are taken into account at each cycle depending on the system periodicity (for example each millisecond). Under certain circumstances this can be insufficient when more accuracy is needed, or if a quick response is required from the system. To fill the gap, a drive may have some Fast Input connections (generally one or two). When an event happens that triggers a Fast Input (e.g. when a sensor sends a rising edge), the detection of a signal occurs faster (which can be 1000 times more accurate than the system periodicity). Then the timestamp associated with this input can be provided to the IPC to take corrective action. - This value is only valid when TrigIsTrigged() returns TRUE.
- The Trigger block extrapolates the output value based on the timestamp
A timestamp is a sequence of characters, denoting the date and/or time at which a certain event occurred of the Fast Input event to provide an accurate position even if the event occurs in the middle of a program cycle.
- The Trigger block extrapolates the output value based on the timestamp
- Once triggered, a block has to be reset before it can be triggered again.
- Modulo Calculation: MLTrigReadPos uses the Output Modulo Position value of the previous block in the pipe, even if the previous pipe is configured for No Modulo mode.
- The previous block must specify a 0 (zero) value for Output Modulo Position before setting the Mode to No Modulo to prevent a modulo operation for MLTrigReadPosPipe.
- Previous Function Name: MLTrigGetPos
Fast Homing - Inputs
See these topics for more information:
- Fast Homing Example with the Pipe Network Motion Engine Axis Pipe Block
- Fast Homing Example with the PLCopen Motion Engine
- Fast Inputs with Pipe Network Motion
- Pipe Network Registration and Fast Homing
- Registration Position Capture Example with Pipe Network Trigger Block
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Save position of Axis when Fast Input event occurs
Trig_Position := MLTrigReadPos( PipeNetwork.TRIGGER );
See Also