MLTrigWriteDelay
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Sets the time the trigger block uses to compensate for the delay introduced by the sensor
A sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer that captures the triggering signal.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
Identifier of the trigger block. |
|
Delay |
LREAL |
No range |
Microseconds |
No default |
Reaction time of the sensor that the trigger block has to compensate. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
No range |
N/A |
Returns TRUE if the delay is successfully set. . See Pipe Network - General Rules for more information. |
Remarks
- Allows the trigger block to calculate the exact moment at which a signal was triggered by the specified compensation.
- The delay compensation should include drive processing time, sensor delay, and the communication latency through the EtherCAT
***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs network. - Electronic sensors are not able to respond immediately to a signal.
- Sensors usually require a certain amount of time to process a change of state in their input signal.
Fast Homing - Inputs
See these topics for more information:
- Fast Homing Example with the Pipe Network Motion Engine Axis Pipe Block
- Fast Homing Example with the PLCopen Motion Engine
- Fast Inputs with Pipe Network Motion
- Pipe Network Registration and Fast Homing
- Registration Position Capture Example with Pipe Network Trigger Block
FBD Language Example
Not available.
FFLD Language Example
Not available.
IL Language Example
Not available.
ST Language Example
Not available.
See Also