CurveLin
Function Block
A function block groups an algorithm and a set of private data. It has inputs and outputs. - Linear interpolation on a curve.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
X |
REAL |
|
|
|
X coordinate of the point to be interpolated. |
|
XAxis |
REAL[ ] |
|
|
|
X coordinates of the known points of the X axis. |
|
YVal |
REAL[ ] |
|
|
|
Y coordinate of the points defined on the X axis. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
ERR |
DINT |
|
|
|
|
OK |
BOOL |
|
|
TRUE if successful. |
|
Y |
REAL |
|
|
Interpolated Y value corresponding to the X input. |
Remarks
- This function performs linear interpolation in between a list of points defined in the XAxis single dimension array.
- The output Y value is an interpolation of the Y values of the two rounding points defined in the X axis.
- Y values of defined points are passed in the YVal single dimension array.
- Values in XAxis must be sorted from the smallest to the biggest.
- There must be at least two points defined in the X axis.
- YVal and XAxis input arrays must have the same dimension.
- There must be at least two points defined in the X axis.
- If the X input is less than the smallest defined X point:
- The Y output takes the first value defined in YVal.
- An error is reported.
- If the X input is greater than the biggest defined X point:
- The Y output takes the last value defined in YVal.
- An error is reported.
If the function fails, the ERR output gives the cause of the error:
|
Error Code |
Meaning |
|---|---|
|
0 |
OK |
|
1 |
Invalid dimension of input arrays |
|
2 |
Invalid points for the X axis |
|
4 |
X is out of the defined X axis |
FBD Language Example
Not available.
FFLD Language Example
Not available.
IL Language Example
Not available.
ST Language Example
Not available.