IF THEN ELSE ELSIF END_IF
Syntax
IF <BOOL expression> THEN
<statements>
ELSIF <BOOL expression> THEN
<statements>
ELSE
<statements>
END_IF;
Remarks
- The IF statement is available in ST
"Structured text"
A high-level language that is block structured and syntactically resembles Pascal only. - The execution of the statements is conditioned by a Boolean expression.
- ELSIF and ELSE statements are optional.
- There can be several ELSIF statements.
FBD Language Example
Not available.
FFLD Language Example
Not available.
IL Language Example
Not available.
ST Language Example
(* simple condition *)
IF bCond THEN
Q1 := IN1;
Q2 := TRUE;
END_IF;
(* binary selection *)
IF bCond THEN
Q1 := IN1;
Q2 := TRUE;
ELSE
Q1 := IN2;
Q2 := FALSE;
END_IF;
(* enumerated conditions *)
IF bCond1 THEN
Q1 := IN1;
ELSIF bCond2 THEN
Q1 := IN2;
ELSIF bCond3 THEN
Q1 := IN3;
ELSE
Q1 := IN4;
END_IF;
See Also