FlipFlop
Function Block
A function block groups an algorithm and a set of private data. It has inputs and outputs. - Flipflop bistable.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN |
BOOL |
|
|
|
Swap command (on rising edge |
|
RST |
BOOL |
|
|
|
Reset to FALSE. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
BOOL |
|
|
Output. |
Remarks
- The output is systematically reset to FALSE if RST is TRUE.
- The output changes on each rising edge of the IN input, if RST is FALSE.
FBD Language Example
FFLD Language Example
IL Language Example
(* MyFlipFlop is declared as an instance of FLIPFLOP function block: *)
Op1: CAL MyFlipFlop (IN, RST)
FFLD"Free Form Ladder Diagram" MyFlipFlop.Q
ST Q1
ST Language Example
(* MyFlipFlop is declared as an instance of FLIPFLOP function block: *)
MyFlipFlop (IN, RST);
Q := MyFlipFlop.Q;
See Also