sema
Function Block
A function block groups an algorithm and a set of private data. It has inputs and outputs. - Semaphore.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
CLAIM |
BOOL |
|
|
|
Takes the semaphore. |
|
RELEASE |
BOOL |
|
|
|
Releases the semaphore. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
BUSY |
BOOL |
|
|
TRUE if semaphore is busy. |
Remarks
The function block implements this algorithm:
BUSY := mem;
if CLAIM then
mem := TRUE;
else if RELEASE then
BUSY := FALSE;
mem := FALSE;
end_if;
FBD Language Example
FFLD Language Example
- In the FFLD
"Free Form Ladder Diagram" Language, the input rung
is the CLAIM command. - The output rung is the BUSY output signal.
IL Language Example
(* MySema is a declared instance of SEMA function block *)
Op1: CAL MySema (CLAIM, RELEASE)
FFLD MyBlinker.BUSY
ST BUSY
ST Language Example
(* MySema is a declared instance of SEMA function block *)
MySema (CLAIM, RELEASE);
BUSY := MyBlinker.BUSY;