DTMin
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Get the minutes from the time stamp.
Inputs
|
Input |
Data Type |
Range | Unit | Default |
Description |
|---|---|---|---|---|---|
|
Time |
DINT |
0 to 86,399,999 |
Milliseconds |
No default |
The number of milliseconds that have passed since midnight. This value is typically retrieved from DTCurTime. |
Outputs
|
Output |
Data Type |
Range | Unit |
Description |
|---|---|---|---|---|
|
Q |
DINT |
0 to 59 |
Minutes |
Minutes of the time. |
Remarks
None
FBD Language Example
Not available.
FFLD Language Example
Not available.
IL Language Example
Not available.
ST Language Example
Q := DTMin (iTime);
See Also