DTSetNTPSync
Function Block
A function block groups an algorithm and a set of private data. It has inputs and outputs. - Set the NTP
"Network Time Protocol"
A networking protocol for clock synchronization between computer systems.
The PCMM2G can be configured to synchronize with public NTP time servers over the internet or a local NTP time server for networks that are not connected to the internet. synchronization enable state.
This function block is specific for PCMM2G only.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Execute |
BOOL |
TRUE, FALSE |
N/A |
No default |
If TRUE, request to set the synchronization enable state. |
|
SynchEn |
BOOL |
TRUE, FALSE |
N/A |
No default |
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Done |
BOOL |
TRUE, FALSE |
N/A |
If TRUE, the command completed successfully. |
|
Error |
BOOL |
TRUE, FALSE |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
DINT |
No range |
N/A |
Indicates the error if the Error output is set to TRUE. Error Codes
|
Remarks
None
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
// enable NTP server synchronization
Inst_DTSetNTPSync( bSetNTPSync, bNTPSyncEnable );
if Inst_DTSetNTPSync.Done then
bSetNTPSync := false;
bError := Inst_DTSetNTPSync.Error;
ErrorID := Inst_DTSetNTPSync.ErrorID;
end_if;
See Also