any_to_int / any_to_uint
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN |
ANY |
|
|
|
Input value. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
INT |
|
|
Value converted to a signed integer. (16-bit). |
|
Q |
UINT |
|
|
Value converted to an unsigned integer. (16-bit). |
Remarks
Can be unsigned with any_to_uint.
Data Type Outputs
- For BOOL input data types, the output is 0 (zero) or 1.
- For REAL input data type, the output is the integer part of the input real.
- For TIME input data types, the output is the number of milliseconds.
- For STRING input data types, the output is the number represented by the string or 0 (zero) if the string does not represent a valid number.
FBD Language Example
FFLD Language Example
- In the FFLD
"Free Form Ladder Diagram" Language, the conversion is executed only if the input rung (EN) is TRUE. - The output rung (ENO) keeps the same value as the input rung.
IL Language Example
- In the IL
"Instruction List"
This is a low-level language and resembles assembly Language, the any_to_int converts the current result.
Op1: FFLD IN
ANY_TO_INT
ST Q
ST Language Example
Q := ANY_TO_INT (IN);
See Also