bcd_to_bin
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Converts a Binary Coded Decimal (BCD) value to a binary value.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN |
DINT |
|
|
|
Integer value in BCD. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
DINT |
|
|
Converts a Binary Coded Decimal (BCD) value to a binary value. Value converted to integer or 0 (zero) if IN is not a valid positive BCD value. |
Remarks
- The input must:
- Be positive.
- Represent a valid BCD value.
Truth Table
|
IN |
Q |
|---|---|
|
-2 |
0 (invalid) |
|
0 |
0 |
|
16 (16#10) |
10 |
|
15 (16#0F) |
0 (invalid) |
FBD Language Example
FFLD Language Example
- In the FFLD
"Free Form Ladder Diagram" Language, the operation is executed only if the input rung (EN) is TRUE. - The output rung (ENO) keeps the same value as the input rung.
IL Language Example
- In the IL
"Instruction List"
This is a low-level language and resembles assembly Language, the input must be loaded in the current result before calling the function.
Op1: LD"Ladder diagram" Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them IN
BCD_TO_BIN
ST Q
ST Language Example
Q := BCD_TO_BIN (IN);
See Also