or_mask
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Performs a bit-to-bit Boolean OR between two integer values.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN |
ANY |
|
|
|
First input. |
|
MSK |
ANY |
|
|
|
Second input. (OR mask) |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
ANY |
|
|
OR mask between IN and MSK inputs. |
Remarks
- Arguments can be signed or unsigned integers from 8- to 32-bits.
FBD Language Example
FFLD Language Example
- In the FFLD
"Free Form Ladder Diagram" Language, the input rung (EN) enables the operation.- The output rung keeps the state of the input rung.
- The function is executed only if EN is TRUE.
- ENO has the same value as EN.
IL Language Example
- In the IL
"Instruction List"
This is a low-level language and resembles assembly Language, the first parameter (IN) must be loaded in the current result before calling the function. - The other input is the operands of the function.
Op1: LD"Ladder diagram" Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them IN
OR_MASK MSK
ST Q
ST Language Example
Q := OR_MASK (IN, MSK);
See Also