LoadString
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Loads a string from the active string table.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
ID |
DINT |
|
|
|
ID of the string as declared in the string table. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
STRING |
|
|
Loaded string or empty string in case of error. |
Remarks
- This function loads a
string from the active string table and stores it in a STRING variable.
- The StringTable function is used for selecting the active string table.
- The ID input (the string item identifier) is an identifier declared within the string table resource.
- You don't need to define this identifier again - the system does it for you.
FBD Language Example
FFLD Language Example
IL Language Example
Op1: LD"Ladder diagram" Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them ID
LoadString
ST Q
ST Language Example
Q := LoadString (ID);
See Also