ATOH
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Converts a string to an integer using hexadecimal basis.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN |
STRING |
|
|
|
String representing an integer in hexadecimal format. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
DINT |
|
|
Integer represented by the string. |
Remarks
- This function is case insensitive.
- The result is 0 (zero) for an empty string.
- The conversion stops before the first invalid character.
Truth Table
|
IN |
Q |
|---|---|
|
'' |
0 |
|
'12' |
18 |
|
'a0' |
160 |
|
'A0zzz' |
160 |
FBD Language Example
FFLD Language Example
- In the FFLD
"Free Form Ladder Diagram" Language, the operation is executed only if the input rung (EN) is TRUE. - The output rung (ENO) keeps the same value as the input rung.
IL Language Example
- In the IL
"Instruction List"
This is a low-level language and resembles assembly Language, the first input must be loaded before the function call.
Op1: LD"Ladder diagram" Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them IN
ATOH
ST Q
ST Language Example
Q := ATOH (IN);
See Also