char
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Builds a single character string.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
CODE |
DINT |
|
|
|
ASCII code of the specified character. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
STRING |
|
|
STRING containing only the specified character. |
Remarks
None
FBD Language Example
FFLD Language Example
- In the FFLD
"Free Form Ladder Diagram" Language, the input rung (EN) enables the operation. - The output rung (ENO) keeps the same value as the input rung.
IL Language Example
- In the IL
"Instruction List"
This is a low-level language and resembles assembly Language, the input parameter (CODE) must be loaded in the current result before calling the function.
Op1: LD"Ladder diagram" Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them CODE
CHAR
ST Q
ST Language Example
Q := CHAR (CODE);
See Also