UseDegrees
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Sets the unit for angles in all trigonometric functions.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN |
BOOL |
|
|
|
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
BOOL |
|
|
TRUE if functions use degrees before the call. |
Remarks
This function sets the working unit for these functions:
|
Function |
Description |
|---|---|
|
Calculate an arc-cosine. |
|
|
Calculate an arc-sine. |
|
|
Calculate an arc-tangent. |
|
|
Calculate arc-tangent of Y/X. |
|
|
Calculate a cosine. |
|
|
Calculate a sine. |
|
|
Calculate a tangent. |
FBD Language Example
FFLD Language Example
- The first input is the rung.
- The rung is the output.
IL Language Example
Op1: LD"Ladder diagram" Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them IN
UseDegrees
ST Q
ST Language Example
Q := UseDegrees (IN);