udpRcvFromArray
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Receives a byte array through UDP
"User Datagram Protocol".
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
En |
BOOL |
0, 1 |
N/A |
No default |
Execute the function. |
|
sock |
DINT |
0, 65535 |
N/A |
No default |
Socket number, return value from udpCreate. |
|
nb |
DINT |
0, 65535 |
N/A |
No default |
Number of bytes to be transferred. |
|
add[ ] |
USINT |
0, 32 |
N/A |
No default |
Array which contains information about the server. |
|
data[ ] |
USINT |
0, 65535 |
N/A |
No default |
Array of bytes to be transferred. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
OK |
BOOL |
|
N/A |
Returns TRUE when the function successfully executes. See Pipe Network - General Rules for more information. |
|
Q |
DINT |
|
N/A |
Number of bytes received. |
Remarks
None
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
BytesReceived := udpRcvFromArray(Socket_Number,nb,add,FrameIn networking dialect, a message is called a frame);