udpSendTo
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Sends a UDP
"User Datagram Protocol" telegram.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
En |
BOOL |
0, 1 |
N/A |
No default |
Execute the function. |
|
sock |
DINT |
0, 65535 |
N/A |
No default |
ID of the client socket. |
|
nb |
DINT |
0, 65535 |
N/A |
No default |
Number of bytes of data to send. |
|
add[ ] |
USINT |
0, 32 |
N/A |
No default |
Buffer containing the UDP address (filled on output). |
|
data |
STRING |
0, 255 |
N/A |
No default |
The characters to send. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
OK |
BOOL |
|
N/A |
Returns TRUE when the function successfully executes. See Pipe Network - General Rules for more information. |
Remarks
None
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
bUdpSendTo := udpSendTo(Socket_Number,5,add,'1000');