NVRAM
KAS uses (missing or bad snippet) to save Retain Variables.
|
Hardware Type |
|
|---|---|
|
Simulator |
256 Kbytes |
|
AKD PDMM or PCMM |
32 Kbytes |
|
PCMM2G |
256 Kbytes |
-
-
Part of (missing or bad snippet) allocation is reserved to store some internal data (144 bytes).
As a consequence, not all of the complete physical (missing or bad snippet) is available for the retain variables.
If the size is big enough, KAS updates the non-volatile memory to store the retain variables values.
- This operation is performed in the background every 20 seconds.
- The frequency increases to every two seconds when the application is running or when you shutdown the application.
(missing or bad snippet) Life Expectancy
- Data Retention: At maximum operating temperature, the data written to the memory is retained for 10 years.
- Endurance: (missing or bad snippet) memory has an endurance limit of 1014 read/write accesses.
- More than 6,000,000 years of being accessed every 2 seconds.
-
-
Using the retain variables is very cycle time consuming.
As a consequence, Kollmorgen strongly recommends to carefully monitor the system load with the TraceTimes command.
Verify the (missing or bad snippet) Space
To calculate (missing or bad snippet) space, add the size of each retained variable according to the:
- Data Types
- Arrays - The numbers of elements in case the variable is declared as an array.
Remember! Add the 144 bytes!
In this example, the total size is: 3684 bits (which is less than 0.5 Kbytes).
|
Variable |
Size / element |
Number of Element |
Total Size / variable |
|---|---|---|---|
|
bLedStatus |
1-bit |
4 |
4 |
|
Internal data |
1152-bits (144 bytes) |
N/A |
1152 |
|
MasterAbsPos |
64-bits |
1 |
64 |
|
MyString |
800-bits (100 bytes) |
3 |
2400 |
|
TravelSpeed |
64-bits |
1 |
64 |