Connect Remotely
You can connect to a controller from an external network using VPN or other tunneling protocol.
You must open these ports which are used by KAS to connect to a controller:
|
80
|
KAS-:
- Controller Web Server
- Download application
- front end communication.
- This is necessary for the connection to the .
- If port 80 is used by any other application, the Simulator uses an alternate port available in the host computer for HTTP communication.
|
|
502
|
and other devices to communicate with Modbus TCP.
|
|
2222
|
EtherNet/IP communication.
|
|
4002
|
KAS-IDE: Oscilloscope variable monitoring.
|
|
4003
|
KAS-IDE:
- Communication with the PLC Virtual Machine.
- This is necessary for the connection to the runtime.
|
|
9900
|
KAS-IDE:
- Communication with the runtime engine; WorkBench views.
- This is necessary for the connection to the runtime.
|
|
34962
|
PROFINET communication.
|
|
34964
|
PROFINET communication.
|
|
44848
|
EtherNet/IP communication.
|