Troubleshooting FSoE Safety Parameters
***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs master (the PCMM or AKD PDMM).
The first thing to do is to check the ErrorID output of FSoEParamsInit. There are some common failure cases that can be identified from the ErrorID values and the Controller log messages.
| ECERR_DEVICE_NOTREADY |
The Safety parameters can only be sent after the EtherCAT network state is in op-mode. To verify EtherCAT is ready:
|
| ECERR_DEVICE_FSOE_MASTER_INVALID |
This error is generated if the argument specified for FSoEParamsInit's FSoEMasterAddress is not a FSOE Master.
|
| ECERR_DEVICE_TIMEOUT |
This can occur if the FSoE Master is not responding or is not configured properly.
|
If FSoeParamsInit(...) is successful but the AKD2G Safety State does not reach 6 - Normal operation then the CRC
"Cyclic redundancy check"
A CRC is a type of function that takes as input a data stream of any length and produces as output a value of a certain fixed size. The term CRC is often used to denote either the function or the function's output. A CRC can be used as a checksum to detect accidental alteration of data during transmission or storage expected by the AKD2G SMM does not match the CRC sent by the FSoE master.
- Use WorkBench or the KAS-IDE
"Integrated development environment"
An integrated development environment is a type of computer software that assists computer programmers in developing software.
IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger's integrated WorkBench (Configuration tab for the AKD2G) to diagnose. - Click the "Safety" item in the status bar.
The AKD2G has two options for configuring safety parameters which are determined by selecting the modules associated with the AKD2G in the KAS-IDE Project Tree.
If the module(s) are set for “Workbench Parameters” then the FSoE Master cannot set the AKD2G’s safety parameters. The "WorkBench Parameter" modules are set by default when the AKD2G is scanned and discovered. The modules must be changed to accept the parameter from the Safety Maser if you want to use FSoEParamsInit. The picture below shows the appropriate modules for using FSoEParamsInit with AKD2G.
Additionally, the AKD2G profile in the SafePLC2 project should be set to "FSx Axis Y" in order to send the parameters to the AKD2G.
This can occur in two situations:
- if the FSoE safety parameters have been previously configured correctly
- if the FSoE Master has not been configured properly.
FSoEParamsInit will only initialize safety parameters if the FSoE master determines there are parameters to set in the safety device(s). Please check the FSoE master configuration using the vendor’s software. For example, with the BBH SCU-1-EC FSoE master, use the SafePLC2 software.
See Also