Motion Control Main Functions

To ensure accurate positioning and movement, motion controlClosed Motion control is a sub-field of automation, in which the position and/or velocity of machines are controlled using some type of device such as a hydraulic pump, linear actuator, or an electric motor, generally a servo. Motion control is an important part of robotics and CNC machine tools; however, it is more complex than in the use of specialized machines, where the kinematics is usually simpler. The latter is often called General Motion Control (GMC). Motion control is widely used in the packaging, printing, textile and assembly industries consists of the two following main parts:

Setpoint Generation

  • This consists of generating a trajectory defined by position versus time.
  • It is purely logical and does not relate to the physical world.

Regulation

Even using the very best drives, you cannot maintain accurate positioning without a feedback loop.

These two functions can be located on the same hardware (as in a "stand-alone" servo driveClosed A servo drive is a special electric amplifier used to power electric servo motors. It monitors feedback signals from the motor and continually adjusts for deviation from expected behavior) or on two separate hardware devices, linked together by a fieldbus.

Regulation with Remote Drive

Figure 9-2: Regulation with Remote Drive

Concept Link IconSee Also