Axis Positions Data
Actual Position
This is the position of the axis read from the drive interface, which is read from the feedback device
A process whereby some proportion of the output signal of a system is passed (fed back) to the input.
In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position.
CommandPosition
This is the command position (without modulo and in the axis' User Units) sent to the drive interface to command an axis.
This position is tied to the Status output of the MC_Power function block:
- Status = 1: The command position is a combination of the Normal, Superimposed, and Phasing commands.
- Status = 0: The command position tracks the Actual Position.
CoordinatedMotionCmdPos
This is the command position generated by the Coordinated Motion Interpolator when interpolating coordinated motion moves.
Group Actual Position
This is the set of positions of an axes group read from the axis interface:
Figure 9-46: How Actual Position is Calculated
NormalCmdPos
This is the command position generated by the Normal Interpolator when interpolating a single axis move or a slave move.
PhaseCmd Pos
This is the command position generated by the Phasing Interpolator when interpolating a MC_Phasing master phase shift.
It is incorporated in the generation of the NormalCmdPos when interpolating a slave move.
SuperimposedCmdPos
This is the command position generated by the Superimposed Interpolator when interpolating a MC_Superimp move
Figure 9-47: Calculated PLCopen Axis Position Data