AXIS_REF Structure

The PLCopenClosed A vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML specification indicates a Structure used for identifying the axis at a function block input.

AXIS_REF contains these members:

Member

Type

Description

AXIS_NUM

INT

The axis number.

AXIS_ENGINE

UINT

Reserved.

Do not modify this variable or rely on its value.

See Modify PLCopen Axis for more information about Axis Number.

You have to create and initialize this data structure in your application.

See Function Blocks Description for more information.

Concept Link IconSee Also