Behavior of Busy Output
The Busy output indicates that the function block is still working, with new output values to be expected.
- Busy is SET at the rising edge A rising edge is the transition of a digital signal from low to high. It is also called positive edge of Execute and RESET when one of the outputs (e.g., Done, Aborted, or Error) is set.
- It is recommended that this function block is kept in the active loop of the application program for at least as long as Busy is TRUE, because the outputs can still change.
- For one axis, several function blocks can be busy, but only one can be active at a time.
- Exceptions are MC_SuperImposed and MC_Phasing, where more than one function block related to one axis can be active.