Active Output
The Active output is set at the moment the function block takes control of the motion of the respective axis.
Coordinated Motion
Use this table to determine the state of the Busy and Active outputs when transitioning from one move to the next.
Function Block Output | First Move | Second Move |
---|---|---|
Busy | False | True |
Active | False | False |
Done | True1 | False |