Intellisense
"Structured text"
A high-level language that is block structured and syntactically resembles Pascal and FBD
"Function Block Diagram"
A function block diagram describes a function between input variables and output variables. A function is described as a set of elementary blocks programs:
-
-
They do not apply to actions in an SFC
"Sequential Function Chart"
It can be used to program processes that can be split into steps.
The main components of SFC are:
- Steps with associated actions
- Transitions with associated logic conditions
- Directed links between steps and transitions step.
Conditional compiling coloring
Parts of conditional compiling code (declared with #ifdef pragmas) that are not validated are grayed
Commenting the CONDITION changes the active part of the program
-
-
Save your project to have the code with the correct colors.
Auto-indentation
Lines are automatically indented on the left when you enter structured ST statements