Redundant PDO Entries
It is possible in the KAS-IDE
"Integrated development environment"
An integrated development environment is a type of computer software that assists computer programmers in developing software.
IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger to have the same PDO
PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. entry occur in multiple PDOs (or even in a single PDO).
- A PDO entry is uniquely defined by an index and a subindex.
- The name of the entry is irrelevant in regards to identification.
In this example:
Redundant Rx PDO
The redundant Rx PDO would generate this compiler error:
EtherCAT: ERROR: In AKD_1, PDO object index 0x6040, subIndex 0 is redundant. It is in the following PDO(s): 0x1600, 0x1604
Attempting to export the ENI file fails with this error:
Failed to export ENI file, check the logs for more details.
Redundant Tx PDO
A redundant Tx PDO entry does not prevent a successful compilation nor generate an error when exporting the ENI file.
A redundant Tx PDO entry generates a compiler warning:
EtherCAT: Warning : In AKD_1, PDO object index 0x3470, subIndex 4 is redundant. It is in the following PDO(s): 0x1A04, 0x1B23