Start the KAS-IDE
There are multiple ways to start the KAS-IDE
"Integrated development environment"
An integrated development environment is a type of computer software that assists computer programmers in developing software.
IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger.
- Double-click a desktop shortcut.
- Double-click a project file to open it with the most recently installed version of the KAS-IDE.
- Windows 10 and 11: From the Start menu, under "K".
- All installed versions are found here, including one legacy version (in the Kollmorgen folder), and all installed versions of v3.01 and later.
- See Can I install more than one version of the KAS-IDE? for more information.

-
- The KAS-IDE supports simultaneously running multiple instances.
Double-click a shortcut or project file, or selecting the application from the Start menu opens another instance.
Double-click a project file more than once opens a copy of the project in another instance of the KAS-IDE.
See the these FAQs for more options: