Booting the AKD PDMM or PCMM Controller
This topic explains the boot sequence for the controller, which is based on the RAM and the Flash memory.
The flash memory contains two images:
- Recovery image (4 Mb) contains QNX operating system and the KAS web server.
- Regular image (9 Mb) contains QNX operating system, the KAS web server, and the KAS Runtime
In computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time).
Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running.
See Also